Package | Description |
---|---|
nxopen.cam |
Provides classes and interfaces for Manufacturing.
|
Modifier and Type | Field and Description |
---|---|
static CornerControlBuilder.SmoothingOptions |
CornerControlBuilder.SmoothingOptions.ALL_PASSES
all passes
|
static CornerControlBuilder.SmoothingOptions |
CornerControlBuilder.SmoothingOptions.NONE
none
|
Modifier and Type | Method and Description |
---|---|
CornerControlBuilder.SmoothingOptions |
CornerControlBuilder.smoothingOption()
Returns the corner smoothing option
License requirements: None. |
static CornerControlBuilder.SmoothingOptions |
CornerControlBuilder.SmoothingOptions.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static CornerControlBuilder.SmoothingOptions |
CornerControlBuilder.SmoothingOptions.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static CornerControlBuilder.SmoothingOptions[] |
CornerControlBuilder.SmoothingOptions.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
CornerControlBuilder.setSmoothingOption(CornerControlBuilder.SmoothingOptions smoothingOption)
License requirements: cam_base ("CAM BASE") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.