Package | Description |
---|---|
nxopen.cam |
Provides classes and interfaces for Manufacturing.
|
Modifier and Type | Field and Description |
---|---|
static ConvertFromMCDBuilder.MachineTypes |
ConvertFromMCDBuilder.MachineTypes.MILL |
static ConvertFromMCDBuilder.MachineTypes |
ConvertFromMCDBuilder.MachineTypes.MILL_TURN |
static ConvertFromMCDBuilder.MachineTypes |
ConvertFromMCDBuilder.MachineTypes.TURN |
Modifier and Type | Method and Description |
---|---|
ConvertFromMCDBuilder.MachineTypes |
ConvertFromMCDBuilder.machineType()
Returns the machine type method
License requirements: None. |
static ConvertFromMCDBuilder.MachineTypes |
ConvertFromMCDBuilder.MachineTypes.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static ConvertFromMCDBuilder.MachineTypes |
ConvertFromMCDBuilder.MachineTypes.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static ConvertFromMCDBuilder.MachineTypes[] |
ConvertFromMCDBuilder.MachineTypes.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
ConvertFromMCDBuilder.setMachineType(ConvertFromMCDBuilder.MachineTypes machineType)
License requirements: ug_isv_full ("Full functionality for Integrated Simulation and Verification") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.