Package | Description |
---|---|
nxopen.cam |
Provides classes and interfaces for Manufacturing.
|
Modifier and Type | Field and Description |
---|---|
static CenterlineDrillTurningBuilder.OutputOptionTypes |
CenterlineDrillTurningBuilder.OutputOptionTypes.MACHINE_CYCLE
Output Option: Machine Cycle
|
static CenterlineDrillTurningBuilder.OutputOptionTypes |
CenterlineDrillTurningBuilder.OutputOptionTypes.SIMULATED
Output Option: Simulated
|
Modifier and Type | Method and Description |
---|---|
CenterlineDrillTurningBuilder.OutputOptionTypes |
CenterlineDrillTurningBuilder.outputOption()
Returns the output option
License requirements: None. |
static CenterlineDrillTurningBuilder.OutputOptionTypes |
CenterlineDrillTurningBuilder.OutputOptionTypes.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static CenterlineDrillTurningBuilder.OutputOptionTypes |
CenterlineDrillTurningBuilder.OutputOptionTypes.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static CenterlineDrillTurningBuilder.OutputOptionTypes[] |
CenterlineDrillTurningBuilder.OutputOptionTypes.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
CenterlineDrillTurningBuilder.setOutputOption(CenterlineDrillTurningBuilder.OutputOptionTypes outputOptionMode)
License requirements: cam_base ("CAM BASE") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.