Package | Description |
---|---|
nxopen.cam |
Provides classes and interfaces for Manufacturing.
|
Modifier and Type | Field and Description |
---|---|
static CenterlineDrillTurningBuilder.DepthTypes |
CenterlineDrillTurningBuilder.DepthTypes.COUNTERSINK_DIAMETER
Depth options: Countersink Diameter
|
static CenterlineDrillTurningBuilder.DepthTypes |
CenterlineDrillTurningBuilder.DepthTypes.CROSS_HOLE
Depth options: Cross Hole
|
static CenterlineDrillTurningBuilder.DepthTypes |
CenterlineDrillTurningBuilder.DepthTypes.CROSS_HOLE_DIMENSIONS
Depth options: Cross Hole Dimensions
|
static CenterlineDrillTurningBuilder.DepthTypes |
CenterlineDrillTurningBuilder.DepthTypes.DISTANCE
Depth options: Distance
|
static CenterlineDrillTurningBuilder.DepthTypes |
CenterlineDrillTurningBuilder.DepthTypes.END_POINT
Depth options: End Point
|
static CenterlineDrillTurningBuilder.DepthTypes |
CenterlineDrillTurningBuilder.DepthTypes.SHOULDER_DEPTH
obsolete Shoulder Depth
|
Modifier and Type | Method and Description |
---|---|
CenterlineDrillTurningBuilder.DepthTypes |
CenterlineDrillTurningBuilder.depthOption()
Returns the depth option
License requirements: None. |
static CenterlineDrillTurningBuilder.DepthTypes |
CenterlineDrillTurningBuilder.DepthTypes.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static CenterlineDrillTurningBuilder.DepthTypes |
CenterlineDrillTurningBuilder.DepthTypes.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static CenterlineDrillTurningBuilder.DepthTypes[] |
CenterlineDrillTurningBuilder.DepthTypes.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
CenterlineDrillTurningBuilder.setDepthOption(CenterlineDrillTurningBuilder.DepthTypes depthOption)
License requirements: cam_base ("CAM BASE") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.