Package | Description |
---|---|
nxopen.cam |
Provides classes and interfaces for Manufacturing.
|
Modifier and Type | Field and Description |
---|---|
static CAMObject.Status |
CAMObject.Status.APPROVED
Object path has been approved as is
|
static CAMObject.Status |
CAMObject.Status.COMPLETE
Object path has been output
|
static CAMObject.Status |
CAMObject.Status.REGEN
Object path must be regenerated
|
static CAMObject.Status |
CAMObject.Status.REPOST
Object path must be post-processed
|
Modifier and Type | Method and Description |
---|---|
CAMObject.Status |
CAMObject.getStatus()
Get the status of the input object.
|
static CAMObject.Status |
CAMObject.Status.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static CAMObject.Status |
CAMObject.Status.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static CAMObject.Status[] |
CAMObject.Status.values()
Returns an array that contains the values for this enum.
|
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.