Package | Description |
---|---|
nxopen.cam |
Provides classes and interfaces for Manufacturing.
|
Modifier and Type | Field and Description |
---|---|
static BoundaryTurnMemberFineFinishCorner.Cleanup |
BoundaryTurnMemberFineFinishCorner.Cleanup.AUTOMATIC |
static BoundaryTurnMemberFineFinishCorner.Cleanup |
BoundaryTurnMemberFineFinishCorner.Cleanup.MANUAL |
static BoundaryTurnMemberFineFinishCorner.Cleanup |
BoundaryTurnMemberFineFinishCorner.Cleanup.NONE |
Modifier and Type | Method and Description |
---|---|
BoundaryTurnMemberFineFinishCorner.Cleanup |
BoundaryTurnMemberFineFinishCorner.cleanupType()
Returns the fine_finish_corner cleanup
License requirements: None. |
static BoundaryTurnMemberFineFinishCorner.Cleanup |
BoundaryTurnMemberFineFinishCorner.Cleanup.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static BoundaryTurnMemberFineFinishCorner.Cleanup |
BoundaryTurnMemberFineFinishCorner.Cleanup.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static BoundaryTurnMemberFineFinishCorner.Cleanup[] |
BoundaryTurnMemberFineFinishCorner.Cleanup.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
BoundaryTurnMemberFineFinishCorner.setCleanupType(BoundaryTurnMemberFineFinishCorner.Cleanup cornerCleanup)
License requirements: cam_base ("CAM BASE") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.