Package | Description |
---|---|
nxopen.cam |
Provides classes and interfaces for Manufacturing.
|
Modifier and Type | Field and Description |
---|---|
static BoundarySet.ToolSideTypes |
BoundarySet.ToolSideTypes.INSIDE_OR_LEFT
inside for closed boundary, or left side for open boundary
|
static BoundarySet.ToolSideTypes |
BoundarySet.ToolSideTypes.OUTSIDE_OR_RIGHT
outside for closed boundary, or right side for open boundary
|
Modifier and Type | Method and Description |
---|---|
BoundarySet.ToolSideTypes |
BoundarySet.toolSide()
Returns the tool side
License requirements: None. |
static BoundarySet.ToolSideTypes |
BoundarySet.ToolSideTypes.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static BoundarySet.ToolSideTypes |
BoundarySet.ToolSideTypes.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static BoundarySet.ToolSideTypes[] |
BoundarySet.ToolSideTypes.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
BoundarySet[] |
Boundary.appendFaceBoundary(TaggedObject face,
boolean ignoreHole,
boolean ignoreIsland,
boolean ignoreChamfer,
BoundarySet.ToolSideTypes toolSide)
Append the face boundary
License requirements: cam_base ("CAM BASE") . |
void |
BoundarySet.setToolSide(BoundarySet.ToolSideTypes newValue)
License requirements: cam_base ("CAM BASE") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.