Package | Description |
---|---|
nxopen.cam |
Provides classes and interfaces for Manufacturing.
|
Modifier and Type | Interface and Description |
---|---|
interface |
BoundaryMillingMemberSet
Represents a boundary member set .
|
interface |
BoundaryTurnMemberSet
Represents a boundary turning member set .
|
Modifier and Type | Method and Description |
---|---|
BoundaryMemberSet |
BoundarySet.createBoundaryMemberSet()
Create an empty boundary member set
License requirements: cam_base ("CAM BASE") . |
BoundaryMemberSet |
BoundaryMemberSetList.findItem(int index)
Returns the object at the input index.
|
BoundaryMemberSet[] |
BoundaryMemberSetList.getContents()
Gets the contents of the entire list
License requirements: None. |
Modifier and Type | Method and Description |
---|---|
void |
BoundaryMemberSetList.append(BoundaryMemberSet object)
Appends an object to the list
License requirements: None. |
void |
BoundaryMemberSetList.append(BoundaryMemberSet[] objects)
Appends a set of objects to the list
License requirements: None. |
void |
BoundaryMemberSetList.erase(BoundaryMemberSet obj)
Erases the object from the list, but does not delete the object.
|
void |
BoundaryMemberSetList.erase(BoundaryMemberSet obj,
ObjectList.DeleteOption deleteOption)
Erases the object from the list.
|
int |
BoundaryMemberSetList.findIndex(BoundaryMemberSet obj)
Finds the index where the input object appears.
|
void |
BoundaryMemberSetList.insert(int location,
BoundaryMemberSet object)
Inserts an object at the specified location
License requirements: None. |
void |
BoundaryMemberSetList.setContents(BoundaryMemberSet[] objects)
Sets the contents of the entire list.
|
void |
BoundaryMemberSetList.swap(BoundaryMemberSet object1,
BoundaryMemberSet object2)
Exchanges the position of two objects inside the list.
|
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.