public static class TurnAvoidanceGohomeBuilder.GohomePointModes extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_POINT
Point is defined by point.
|
static int |
_SAME_AS_FROM
Point is locked to from point.
|
static TurnAvoidanceGohomeBuilder.GohomePointModes |
POINT
Point is defined by point.
|
static TurnAvoidanceGohomeBuilder.GohomePointModes |
SAME_AS_FROM
Point is locked to from point.
|
Modifier and Type | Method and Description |
---|---|
static TurnAvoidanceGohomeBuilder.GohomePointModes |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static TurnAvoidanceGohomeBuilder.GohomePointModes |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static TurnAvoidanceGohomeBuilder.GohomePointModes[] |
values()
Returns an array that contains the values for this enum.
|
public static final TurnAvoidanceGohomeBuilder.GohomePointModes POINT
public static final TurnAvoidanceGohomeBuilder.GohomePointModes SAME_AS_FROM
public static final int _POINT
public static final int _SAME_AS_FROM
public static TurnAvoidanceGohomeBuilder.GohomePointModes valueOf(int value)
public static TurnAvoidanceGohomeBuilder.GohomePointModes valueOf(String name)
public static TurnAvoidanceGohomeBuilder.GohomePointModes[] values()
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.