public static class NcmWedmBuilder.LeadOutSameAsLeadInTypes extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_NO
not the same
|
static int |
_YES
the same as lead in
|
static NcmWedmBuilder.LeadOutSameAsLeadInTypes |
NO
not the same
|
static NcmWedmBuilder.LeadOutSameAsLeadInTypes |
YES
the same as lead in
|
Modifier and Type | Method and Description |
---|---|
static NcmWedmBuilder.LeadOutSameAsLeadInTypes |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static NcmWedmBuilder.LeadOutSameAsLeadInTypes |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static NcmWedmBuilder.LeadOutSameAsLeadInTypes[] |
values()
Returns an array that contains the values for this enum.
|
public static final NcmWedmBuilder.LeadOutSameAsLeadInTypes NO
public static final NcmWedmBuilder.LeadOutSameAsLeadInTypes YES
public static final int _NO
public static final int _YES
public static NcmWedmBuilder.LeadOutSameAsLeadInTypes valueOf(int value)
public static NcmWedmBuilder.LeadOutSameAsLeadInTypes valueOf(String name)
public static NcmWedmBuilder.LeadOutSameAsLeadInTypes[] values()
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.