public static class InspectionToleranceOperationBuilder.AngleFormat extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_DECIMAL_DEGREE
Decimal Degrees
|
static int |
_DEG_MIN_SEC
Degrees/Minutes/Seconds
|
static InspectionToleranceOperationBuilder.AngleFormat |
DECIMAL_DEGREE
Decimal Degrees
|
static InspectionToleranceOperationBuilder.AngleFormat |
DEG_MIN_SEC
Degrees/Minutes/Seconds
|
Modifier and Type | Method and Description |
---|---|
static InspectionToleranceOperationBuilder.AngleFormat |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static InspectionToleranceOperationBuilder.AngleFormat |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static InspectionToleranceOperationBuilder.AngleFormat[] |
values()
Returns an array that contains the values for this enum.
|
public static final InspectionToleranceOperationBuilder.AngleFormat DECIMAL_DEGREE
public static final InspectionToleranceOperationBuilder.AngleFormat DEG_MIN_SEC
public static final int _DECIMAL_DEGREE
public static final int _DEG_MIN_SEC
public static InspectionToleranceOperationBuilder.AngleFormat valueOf(int value)
public static InspectionToleranceOperationBuilder.AngleFormat valueOf(String name)
public static InspectionToleranceOperationBuilder.AngleFormat[] values()
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.