public static class InspectionOperationTransformBuilder.Line extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_POINT_AND_VECTOR
specify a line by a point and a vector
|
static int |
_SPECIFY
specify a line
|
static int |
_TWO_POINT
specify a line by two point
|
static InspectionOperationTransformBuilder.Line |
POINT_AND_VECTOR
specify a line by a point and a vector
|
static InspectionOperationTransformBuilder.Line |
SPECIFY
specify a line
|
static InspectionOperationTransformBuilder.Line |
TWO_POINT
specify a line by two point
|
Modifier and Type | Method and Description |
---|---|
static InspectionOperationTransformBuilder.Line |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static InspectionOperationTransformBuilder.Line |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static InspectionOperationTransformBuilder.Line[] |
values()
Returns an array that contains the values for this enum.
|
public static final InspectionOperationTransformBuilder.Line SPECIFY
public static final InspectionOperationTransformBuilder.Line TWO_POINT
public static final InspectionOperationTransformBuilder.Line POINT_AND_VECTOR
public static final int _SPECIFY
public static final int _TWO_POINT
public static final int _POINT_AND_VECTOR
public static InspectionOperationTransformBuilder.Line valueOf(int value)
public static InspectionOperationTransformBuilder.Line valueOf(String name)
public static InspectionOperationTransformBuilder.Line[] values()
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.