public static class InspectionLinearMoveToPointBuilder.PointTypeEnums extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_DELTA_XYZ
Enter in a delta value from a point
|
static int |
_EXISTING_POINT
Select an existing point
|
static int |
_POINT_CONSTRUCTOR
Use the Point Constructor
|
static InspectionLinearMoveToPointBuilder.PointTypeEnums |
DELTA_XYZ
Enter in a delta value from a point
|
static InspectionLinearMoveToPointBuilder.PointTypeEnums |
EXISTING_POINT
Select an existing point
|
static InspectionLinearMoveToPointBuilder.PointTypeEnums |
POINT_CONSTRUCTOR
Use the Point Constructor
|
Modifier and Type | Method and Description |
---|---|
static InspectionLinearMoveToPointBuilder.PointTypeEnums |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static InspectionLinearMoveToPointBuilder.PointTypeEnums |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static InspectionLinearMoveToPointBuilder.PointTypeEnums[] |
values()
Returns an array that contains the values for this enum.
|
public static final InspectionLinearMoveToPointBuilder.PointTypeEnums EXISTING_POINT
public static final InspectionLinearMoveToPointBuilder.PointTypeEnums DELTA_XYZ
public static final InspectionLinearMoveToPointBuilder.PointTypeEnums POINT_CONSTRUCTOR
public static final int _EXISTING_POINT
public static final int _DELTA_XYZ
public static final int _POINT_CONSTRUCTOR
public static InspectionLinearMoveToPointBuilder.PointTypeEnums valueOf(int value)
public static InspectionLinearMoveToPointBuilder.PointTypeEnums valueOf(String name)
public static InspectionLinearMoveToPointBuilder.PointTypeEnums[] values()
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.