public static class GrooveToolBuilder.HolderStyles extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_DEG0
0 degrees
|
static int |
_DEG45
45 degrees
|
static int |
_DEG90
90 degrees
|
static int |
_USER_DEFINED
user defined
|
static GrooveToolBuilder.HolderStyles |
DEG0
0 degrees
|
static GrooveToolBuilder.HolderStyles |
DEG45
45 degrees
|
static GrooveToolBuilder.HolderStyles |
DEG90
90 degrees
|
static GrooveToolBuilder.HolderStyles |
USER_DEFINED
user defined
|
Modifier and Type | Method and Description |
---|---|
static GrooveToolBuilder.HolderStyles |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static GrooveToolBuilder.HolderStyles |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static GrooveToolBuilder.HolderStyles[] |
values()
Returns an array that contains the values for this enum.
|
public static final GrooveToolBuilder.HolderStyles DEG0
public static final GrooveToolBuilder.HolderStyles DEG45
public static final GrooveToolBuilder.HolderStyles DEG90
public static final GrooveToolBuilder.HolderStyles USER_DEFINED
public static final int _DEG0
public static final int _DEG45
public static final int _DEG90
public static final int _USER_DEFINED
public static GrooveToolBuilder.HolderStyles valueOf(int value)
public static GrooveToolBuilder.HolderStyles valueOf(String name)
public static GrooveToolBuilder.HolderStyles[] values()
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.