public interface DrillSurfaceBuilder extends TaggedObject
Modifier and Type | Interface and Description |
---|---|
static class |
DrillSurfaceBuilder.SurfaceType
Drill surface type
|
Modifier and Type | Method and Description |
---|---|
void |
setSurface(NXObject surface)
License requirements: cam_base ("CAM BASE") . |
void |
setSurfaceOption(DrillSurfaceBuilder.SurfaceType surfaceOption)
License requirements: cam_base ("CAM BASE") . |
void |
setZcConstant(double zcConstant)
License requirements: cam_base ("CAM BASE") . |
NXObject |
surface()
Returns the selected surface,surface entity type covers Xform,Plane and Face
License requirements: None. |
DrillSurfaceBuilder.SurfaceType |
surfaceOption()
Returns the surface option
License requirements: None. |
double |
zcConstant()
Returns the zc constant, will create one plane based on this value
License requirements: None. |
printTestData, printTestData, tag, tagValue
DrillSurfaceBuilder.SurfaceType surfaceOption() throws NXException, RemoteException
NXException
RemoteException
void setSurfaceOption(DrillSurfaceBuilder.SurfaceType surfaceOption) throws NXException, RemoteException
surfaceOption
- NXException
RemoteException
NXObject surface() throws NXException, RemoteException
NXException
RemoteException
void setSurface(NXObject surface) throws NXException, RemoteException
surface
- entity type can be XFORM, PLANE or FACE.If surface type is PLANE, zcConstant value also is changed based on itNXException
RemoteException
double zcConstant() throws NXException, RemoteException
NXException
RemoteException
void setZcConstant(double zcConstant) throws NXException, RemoteException
zcConstant
- NXException
RemoteException
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.