public static class DmRotaryFloorFinishBuilder.DmSurfCutStepTypes extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_POINTS
Number
|
static int |
_TOLERANCE
Tolerances
|
static DmRotaryFloorFinishBuilder.DmSurfCutStepTypes |
POINTS
Number
|
static DmRotaryFloorFinishBuilder.DmSurfCutStepTypes |
TOLERANCE
Tolerances
|
Modifier and Type | Method and Description |
---|---|
static DmRotaryFloorFinishBuilder.DmSurfCutStepTypes |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static DmRotaryFloorFinishBuilder.DmSurfCutStepTypes |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static DmRotaryFloorFinishBuilder.DmSurfCutStepTypes[] |
values()
Returns an array that contains the values for this enum.
|
public static final DmRotaryFloorFinishBuilder.DmSurfCutStepTypes TOLERANCE
public static final DmRotaryFloorFinishBuilder.DmSurfCutStepTypes POINTS
public static final int _TOLERANCE
public static final int _POINTS
public static DmRotaryFloorFinishBuilder.DmSurfCutStepTypes valueOf(int value)
public static DmRotaryFloorFinishBuilder.DmSurfCutStepTypes valueOf(String name)
public static DmRotaryFloorFinishBuilder.DmSurfCutStepTypes[] values()
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.