public static class DmAmBuilder.AmCustomStartTypes extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_AUTOMATIC
Area Milling Custom Start Automatic
|
static int |
_CUSTOM
Area Milling Custom Start Custom
|
static DmAmBuilder.AmCustomStartTypes |
AUTOMATIC
Area Milling Custom Start Automatic
|
static DmAmBuilder.AmCustomStartTypes |
CUSTOM
Area Milling Custom Start Custom
|
Modifier and Type | Method and Description |
---|---|
static DmAmBuilder.AmCustomStartTypes |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static DmAmBuilder.AmCustomStartTypes |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static DmAmBuilder.AmCustomStartTypes[] |
values()
Returns an array that contains the values for this enum.
|
public static final DmAmBuilder.AmCustomStartTypes CUSTOM
public static final DmAmBuilder.AmCustomStartTypes AUTOMATIC
public static final int _CUSTOM
public static final int _AUTOMATIC
public static DmAmBuilder.AmCustomStartTypes valueOf(int value)
public static DmAmBuilder.AmCustomStartTypes valueOf(String name)
public static DmAmBuilder.AmCustomStartTypes[] values()
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.