public static class CAMSetup.PostprocessSettingsOutputWarning extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_NO
not output the warning file
|
static int |
_POST_DEFINED
use post defined setting
|
static int |
_YES
output the warning file
|
static CAMSetup.PostprocessSettingsOutputWarning |
NO
not output the warning file
|
static CAMSetup.PostprocessSettingsOutputWarning |
POST_DEFINED
use post defined setting
|
static CAMSetup.PostprocessSettingsOutputWarning |
YES
output the warning file
|
Modifier and Type | Method and Description |
---|---|
static CAMSetup.PostprocessSettingsOutputWarning |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static CAMSetup.PostprocessSettingsOutputWarning |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static CAMSetup.PostprocessSettingsOutputWarning[] |
values()
Returns an array that contains the values for this enum.
|
public static final CAMSetup.PostprocessSettingsOutputWarning YES
public static final CAMSetup.PostprocessSettingsOutputWarning NO
public static final CAMSetup.PostprocessSettingsOutputWarning POST_DEFINED
public static final int _YES
public static final int _NO
public static final int _POST_DEFINED
public static CAMSetup.PostprocessSettingsOutputWarning valueOf(int value)
public static CAMSetup.PostprocessSettingsOutputWarning valueOf(String name)
public static CAMSetup.PostprocessSettingsOutputWarning[] values()
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.