Package | Description |
---|---|
nxopen.cae.responsesimulation |
Provides classes and interfaces for Response Simulation.
|
Modifier and Type | Field and Description |
---|---|
static NodalFunctionEvalShellLocation |
NodalFunctionEvalShellLocation.ALL
All three layers
|
static NodalFunctionEvalShellLocation |
NodalFunctionEvalShellLocation.BOTTOM
Bottom layer
|
static NodalFunctionEvalShellLocation |
NodalFunctionEvalShellLocation.MIDDLE
Middle layer
|
static NodalFunctionEvalShellLocation |
NodalFunctionEvalShellLocation.TOP
Top layer
|
Modifier and Type | Method and Description |
---|---|
NodalFunctionEvalShellLocation |
NodalFunctionEvaluationSettingBuilder.shellDataLocation()
Returns the evaluation location of shell element, which is available when
nxopen.cae.responsesimulation and nxopen.cae.responsesimulation is
EvaluationResultType.STRESS , or
EvaluationResultType.STRAIN
License requirements: nx_response_anlys ("NX Response Analysis") Created in NX9.0.0 |
static NodalFunctionEvalShellLocation |
NodalFunctionEvalShellLocation.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static NodalFunctionEvalShellLocation |
NodalFunctionEvalShellLocation.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static NodalFunctionEvalShellLocation[] |
NodalFunctionEvalShellLocation.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
NodalFunctionEvaluationSettingBuilder.setShellDataLocation(NodalFunctionEvalShellLocation shellLocation)
License requirements: nx_response_anlys ("NX Response Analysis") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.