Package | Description |
---|---|
nxopen.cae.responsesimulation |
Provides classes and interfaces for Response Simulation.
|
Modifier and Type | Interface and Description |
---|---|
interface |
CsdEvaluationSetting
Represents the class of evaluation setting for CSD
To create or edit an instance of this class, use CsdEvaluationSettingBuilder Created in NX6.0.0 |
interface |
ElementalFunctionEvaluationSetting
Represents the parameters setting for elemental function evaluation.
|
interface |
FrfEvaluationSetting
Represents the parameters setting for FRF results evaluation
To create or edit an instance of this class, use FrfEvaluationSettingBuilder Created in NX5.0.0 |
interface |
ModalResultsEvaluationSetting
Represents the abstract class of evaluation setting for FRF and transmissibility
This is an abstract class, and cannot be created. |
interface |
NodalFunctionEvaluationSetting
Represents the parameters setting of nodal function response evaluation.
|
interface |
TransmissibilityEvaluationSetting
Represents parameters setting for transmissibility evaluation
To create or edit an instance of this class, use TransmissibilityEvaluationSettingBuilder Created in NX5.0.0 |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.