Package | Description |
---|---|
nxopen.cae.responsesimulation |
Provides classes and interfaces for Response Simulation.
|
Modifier and Type | Interface and Description |
---|---|
interface |
CSDExcitation
Represents an CSD excitation.
|
interface |
DDAMExcitation
Represents an DDAM excitation.
|
interface |
DistributedLoadExcitation
Represents an excitation of distributed-load type
To create or edit an instance of this class, use DistributedLoadExcitationBuilder Created in NX5.0.0 |
interface |
NodalFunctionExcitation
Represents the abstract class of nodal function excitation
This is an abstract class, and cannot be created. |
interface |
RotationalDDAMExcitation
Represents an DDAM excitation.
|
interface |
RotationalNodalFunctionExcitation
Represents a rotational nodal function excitation
To create or edit an instance of this class, use RotationalNodalFunctionExcitationBuilder Created in NX5.0.0 |
interface |
StaticLoadExcitation
Represents an excitation of static load type
To create or edit an instance of this class, use StaticLoadExcitationBuilder Created in NX6.0.0 |
interface |
TranslationalDDAMExcitation
Represents an DDAM excitation.
|
interface |
TranslationalNodalFunctionExcitation
Represents a translational nodal function excitation
To create or edit an instance of this class, use TranslationalNodalFunctionExcitationBuilder Created in NX5.0.0 |
interface |
VelocityImpactExcitation
Represents a velocity impact excitation
To create or edit an instance of this class, use VelocityImpactExcitationBuilder Created in NX6.0.0 |
Modifier and Type | Field and Description |
---|---|
Excitation |
CSDExcitationBuilder.CSDFunction.fromexcitation |
Modifier and Type | Method and Description |
---|---|
Excitation |
ExcitationCollection.findObject(String name)
Finds an excitation with specified excitation name
License requirements: nx_response_anlys ("NX Response Analysis") . |
Excitation[] |
RSEvent.getExcitations()
Returns all excitations of an event
License requirements: nx_response_anlys ("NX Response Analysis") . |
Modifier and Type | Method and Description |
---|---|
void |
ExcitationCollection.deleteExcitation(Excitation excitation)
Deletes an excitation
License requirements: nx_response_anlys ("NX Response Analysis") . |
void |
CSDExcitationBuilder.setFromFunction(Excitation fromExcitation,
Excitation.Component componentType)
Sets the from function
License requirements: nx_response_anlys ("NX Response Analysis") . |
void |
CSDExcitationBuilder.setToFunction(Excitation toExcitation,
Excitation.Component componentType)
Sets the to function
License requirements: nx_response_anlys ("NX Response Analysis") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.