public class StrengthStressCriteria extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_MAX_PRINCIPLE |
static int |
_MIN_PRINCIPLE |
static int |
_VON_MISES |
static StrengthStressCriteria |
MAX_PRINCIPLE |
static StrengthStressCriteria |
MIN_PRINCIPLE |
static StrengthStressCriteria |
VON_MISES |
Modifier and Type | Method and Description |
---|---|
static StrengthStressCriteria |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static StrengthStressCriteria |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static StrengthStressCriteria[] |
values()
Returns an array that contains the values for this enum.
|
public static final StrengthStressCriteria VON_MISES
public static final StrengthStressCriteria MAX_PRINCIPLE
public static final StrengthStressCriteria MIN_PRINCIPLE
public static final int _VON_MISES
public static final int _MAX_PRINCIPLE
public static final int _MIN_PRINCIPLE
public static StrengthStressCriteria valueOf(int value)
public static StrengthStressCriteria valueOf(String name)
public static StrengthStressCriteria[] values()
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.