public static class DDAMExcitation.CoefficientDefinitionType extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_BY_FILE
Get the DDAM coefficients from a DDAM coefficient file
|
static int |
_INPUT_MANUALLY
Input the DDAM coefficient manually
|
static DDAMExcitation.CoefficientDefinitionType |
BY_FILE
Get the DDAM coefficients from a DDAM coefficient file
|
static DDAMExcitation.CoefficientDefinitionType |
INPUT_MANUALLY
Input the DDAM coefficient manually
|
Modifier and Type | Method and Description |
---|---|
static DDAMExcitation.CoefficientDefinitionType |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static DDAMExcitation.CoefficientDefinitionType |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static DDAMExcitation.CoefficientDefinitionType[] |
values()
Returns an array that contains the values for this enum.
|
public static final DDAMExcitation.CoefficientDefinitionType BY_FILE
public static final DDAMExcitation.CoefficientDefinitionType INPUT_MANUALLY
public static final int _BY_FILE
public static final int _INPUT_MANUALLY
public static DDAMExcitation.CoefficientDefinitionType valueOf(int value)
public static DDAMExcitation.CoefficientDefinitionType valueOf(String name)
public static DDAMExcitation.CoefficientDefinitionType[] values()
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.