Package | Description |
---|---|
nxopen.cae.optimization |
Provides classes and interfaces relating to Optimization.
|
Modifier and Type | Field and Description |
---|---|
static TBSTopologyRestrictAreaBuilder.CheckTypeOption |
TBSTopologyRestrictAreaBuilder.CheckTypeOption.CAST
Manufacturing restrictions to guarantee the manufacturing of the elements
|
static TBSTopologyRestrictAreaBuilder.CheckTypeOption |
TBSTopologyRestrictAreaBuilder.CheckTypeOption.FROZEN
All elements of the element group which do not undergo any
changes during optimization
|
static TBSTopologyRestrictAreaBuilder.CheckTypeOption |
TBSTopologyRestrictAreaBuilder.CheckTypeOption.LINK_TOPO
Definition of symmetry and link condtions
|
static TBSTopologyRestrictAreaBuilder.CheckTypeOption |
TBSTopologyRestrictAreaBuilder.CheckTypeOption.MAXIMUMS_SIZE
Defition of the maximum structural diameter
|
static TBSTopologyRestrictAreaBuilder.CheckTypeOption |
TBSTopologyRestrictAreaBuilder.CheckTypeOption.MINIMUM_SIZE
Definition of minimum structural diameter
|
Modifier and Type | Method and Description |
---|---|
TBSTopologyRestrictAreaBuilder.CheckTypeOption |
TBSTopologyRestrictAreaBuilder.checkingType()
Returns the checking type
License requirements: None. |
static TBSTopologyRestrictAreaBuilder.CheckTypeOption |
TBSTopologyRestrictAreaBuilder.CheckTypeOption.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static TBSTopologyRestrictAreaBuilder.CheckTypeOption |
TBSTopologyRestrictAreaBuilder.CheckTypeOption.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static TBSTopologyRestrictAreaBuilder.CheckTypeOption[] |
TBSTopologyRestrictAreaBuilder.CheckTypeOption.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
TBSTopologyRestrictAreaBuilder.setCheckingType(TBSTopologyRestrictAreaBuilder.CheckTypeOption checkType)
License requirements: cae_opt_topo ("NX Topology Optimization") OR cae_opt_topobead ("NX Bead Optimization") OR cae_opt_toposhape ("NX Shape Optimization") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.