Package | Description |
---|---|
nxopen.cae.optimization |
Provides classes and interfaces relating to Optimization.
|
Modifier and Type | Field and Description |
---|---|
static TBSTopologyLinkCondition.AxisType |
TBSTopologyLinkCondition.AxisType.X
Represents X axis
|
static TBSTopologyLinkCondition.AxisType |
TBSTopologyLinkCondition.AxisType.Y
Represents Y axis
|
static TBSTopologyLinkCondition.AxisType |
TBSTopologyLinkCondition.AxisType.Z
Represents Z axis
|
Modifier and Type | Method and Description |
---|---|
TBSTopologyLinkCondition.AxisType |
TBSTopologyLinkCondition.axis()
Returns the axis of symmetry coordinate system
License requirements: None. |
static TBSTopologyLinkCondition.AxisType |
TBSTopologyLinkCondition.AxisType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static TBSTopologyLinkCondition.AxisType |
TBSTopologyLinkCondition.AxisType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static TBSTopologyLinkCondition.AxisType[] |
TBSTopologyLinkCondition.AxisType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
TBSTopologyLinkCondition.setAxis(TBSTopologyLinkCondition.AxisType axis)
License requirements: cae_opt_topo ("NX Topology Optimization") OR cae_opt_topobead ("NX Bead Optimization") OR cae_opt_toposhape ("NX Shape Optimization") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.