Package | Description |
---|---|
nxopen.cae.optimization |
Provides classes and interfaces relating to Optimization.
|
Modifier and Type | Field and Description |
---|---|
static TBSTopologyControllerOptimizationParameters.Speed |
TBSTopologyControllerOptimizationParameters.Speed.FAST
Fast large step size
|
static TBSTopologyControllerOptimizationParameters.Speed |
TBSTopologyControllerOptimizationParameters.Speed.ITERATION
Step size is modified dynamically so the optimization end after the given number of iterations
|
static TBSTopologyControllerOptimizationParameters.Speed |
TBSTopologyControllerOptimizationParameters.Speed.MEDIUM
Medium stepsize
|
static TBSTopologyControllerOptimizationParameters.Speed |
TBSTopologyControllerOptimizationParameters.Speed.MODERATE
Moderate stepsize
|
static TBSTopologyControllerOptimizationParameters.Speed |
TBSTopologyControllerOptimizationParameters.Speed.SLOW
Small stepsize
|
static TBSTopologyControllerOptimizationParameters.Speed |
TBSTopologyControllerOptimizationParameters.Speed.VERY_SLOW
Very small stepsize
|
Modifier and Type | Method and Description |
---|---|
TBSTopologyControllerOptimizationParameters.Speed |
TBSTopologyControllerOptimizationParameters.speedOption()
Returns the speed size of increment
License requirements: None. |
static TBSTopologyControllerOptimizationParameters.Speed |
TBSTopologyControllerOptimizationParameters.Speed.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static TBSTopologyControllerOptimizationParameters.Speed |
TBSTopologyControllerOptimizationParameters.Speed.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static TBSTopologyControllerOptimizationParameters.Speed[] |
TBSTopologyControllerOptimizationParameters.Speed.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
TBSTopologyControllerOptimizationParameters.setSpeedOption(TBSTopologyControllerOptimizationParameters.Speed speedOption)
License requirements: cae_opt_topo ("NX Topology Optimization") OR cae_opt_topobead ("NX Bead Optimization") OR cae_opt_toposhape ("NX Shape Optimization") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.