Package | Description |
---|---|
nxopen.cae.optimization |
Provides classes and interfaces relating to Optimization.
|
Modifier and Type | Field and Description |
---|---|
static TBSSmoothBuilder.IsoType |
TBSSmoothBuilder.IsoType.BOTH
Saves the complete surface
|
static TBSSmoothBuilder.IsoType |
TBSSmoothBuilder.IsoType.NEW
Saves the surface gererated by Isocut
|
static TBSSmoothBuilder.IsoType |
TBSSmoothBuilder.IsoType.ORIGINAL
Saves the original surface
|
Modifier and Type | Method and Description |
---|---|
TBSSmoothBuilder.IsoType |
TBSSmoothBuilder.isoTypeOption()
Returns the option that specifies what should be saved to the output files
License requirements: None. |
static TBSSmoothBuilder.IsoType |
TBSSmoothBuilder.IsoType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static TBSSmoothBuilder.IsoType |
TBSSmoothBuilder.IsoType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static TBSSmoothBuilder.IsoType[] |
TBSSmoothBuilder.IsoType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
TBSSmoothBuilder.setIsoTypeOption(TBSSmoothBuilder.IsoType isoTypeOption)
License requirements: cae_opt_topo ("NX Topology Optimization") OR cae_opt_topobead ("NX Bead Optimization") OR cae_opt_toposhape ("NX Shape Optimization") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.