Package | Description |
---|---|
nxopen.cae |
Provides classes and interfaces relating to Advanced Simulation and Design Simulation.
|
nxopen.cae.optimization |
Provides classes and interfaces relating to Optimization.
|
Modifier and Type | Method and Description |
---|---|
SolutionResult |
ResultManager.createTbsOptimizationSolutionResult(TBSOptimizationSolution tbsOptimizationSolution)
Creates a solution result object given a
TBSOptimizationSolution
It is user's responsibility to destroy the result object once done
using ResultManager.deleteResult(nxopen.cae.Result) , in order to free up system resources
License requirements: nx_masterfem ("Finite Element Modeling") OR nx_design_sim ("NX Design Simulation") Created in NX8.0.1 |
Modifier and Type | Interface and Description |
---|---|
interface |
TBSShapeOptimizationSolution
Represents a shape optimization solution
To create or edit an instance of this class, use TBSShapeOptimizationSolutionBuilder Created in NX8.5.0 |
interface |
TBSTopologyOptimizationSolution
Represents the topology optimization solution
To create or edit an instance of this class, use TBSTopologyOptimizationSolutionBuilder Created in NX8.0.0 |
Modifier and Type | Method and Description |
---|---|
TBSOptimizationSolution |
TBSOptimizationSolutionCollection.cloneSolution(TBSOptimizationSolution sourceSolution,
boolean cloneResult)
Clones an optimization solution and the associated result file optional
License requirements: cae_opt_topo ("NX Topology Optimization") OR cae_opt_topobead ("NX Bead Optimization") OR cae_opt_toposhape ("NX Shape Optimization") . |
TBSOptimizationSolution |
TBSOptimizationSolutionCollection.findObject(String solutionName)
Finds an optimization solution with specified name
License requirements: cae_opt_topo ("NX Topology Optimization") OR cae_opt_topobead ("NX Bead Optimization") OR cae_opt_toposhape ("NX Shape Optimization") . |
Modifier and Type | Method and Description |
---|---|
TBSOptimizationSolution |
TBSOptimizationSolutionCollection.cloneSolution(TBSOptimizationSolution sourceSolution,
boolean cloneResult)
Clones an optimization solution and the associated result file optional
License requirements: cae_opt_topo ("NX Topology Optimization") OR cae_opt_topobead ("NX Bead Optimization") OR cae_opt_toposhape ("NX Shape Optimization") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.