Package | Description |
---|---|
nxopen.cae.optimization |
Provides classes and interfaces relating to Optimization.
|
Modifier and Type | Field and Description |
---|---|
static TBSOptimizationSolution.ResultStatus |
TBSOptimizationSolution.ResultStatus.INVALID
The result is invalid
|
static TBSOptimizationSolution.ResultStatus |
TBSOptimizationSolution.ResultStatus.OUT_OF_DATE
The result is out-of-date
|
TBSOptimizationSolution.ResultStatus |
TBSOptimizationSolution.JA_CAE_OPT_SOL_get_result.status |
static TBSOptimizationSolution.ResultStatus |
TBSOptimizationSolution.ResultStatus.VALID
The result is valid
|
Modifier and Type | Method and Description |
---|---|
static TBSOptimizationSolution.ResultStatus |
TBSOptimizationSolution.ResultStatus.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static TBSOptimizationSolution.ResultStatus |
TBSOptimizationSolution.ResultStatus.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static TBSOptimizationSolution.ResultStatus[] |
TBSOptimizationSolution.ResultStatus.values()
Returns an array that contains the values for this enum.
|
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.