Package | Description |
---|---|
nxopen.cae.optimization |
Provides classes and interfaces relating to Optimization.
|
Modifier and Type | Field and Description |
---|---|
static TBSConstraintBuilder.MagnitudeType |
TBSConstraintBuilder.MagnitudeType.ABSOLUTE
Constraints could be given in absolute values
|
static TBSConstraintBuilder.MagnitudeType |
TBSConstraintBuilder.MagnitudeType.RELATIVE
Constraints could be given in relative values
|
Modifier and Type | Method and Description |
---|---|
TBSConstraintBuilder.MagnitudeType |
TBSConstraintBuilder.magnitude()
Returns the magnitude type of the constraint
License requirements: None. |
static TBSConstraintBuilder.MagnitudeType |
TBSConstraintBuilder.MagnitudeType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static TBSConstraintBuilder.MagnitudeType |
TBSConstraintBuilder.MagnitudeType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static TBSConstraintBuilder.MagnitudeType[] |
TBSConstraintBuilder.MagnitudeType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
TBSConstraintBuilder.setMagnitude(TBSConstraintBuilder.MagnitudeType magnitude)
License requirements: cae_opt_topo ("NX Topology Optimization") OR cae_opt_topobead ("NX Bead Optimization") OR cae_opt_toposhape ("NX Shape Optimization") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.