public static class TBSSmoothBuilder.SelfIntersectionCheckingOption extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_CHECK
Check once
|
static int |
_ITERATIVE
First run without check, then rerun if self-intersections are found
|
static int |
_OFF
No checks
|
static int |
_RUNTIME
Check always
|
static TBSSmoothBuilder.SelfIntersectionCheckingOption |
CHECK
Check once
|
static TBSSmoothBuilder.SelfIntersectionCheckingOption |
ITERATIVE
First run without check, then rerun if self-intersections are found
|
static TBSSmoothBuilder.SelfIntersectionCheckingOption |
OFF
No checks
|
static TBSSmoothBuilder.SelfIntersectionCheckingOption |
RUNTIME
Check always
|
Modifier and Type | Method and Description |
---|---|
static TBSSmoothBuilder.SelfIntersectionCheckingOption |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static TBSSmoothBuilder.SelfIntersectionCheckingOption |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static TBSSmoothBuilder.SelfIntersectionCheckingOption[] |
values()
Returns an array that contains the values for this enum.
|
public static final TBSSmoothBuilder.SelfIntersectionCheckingOption OFF
public static final TBSSmoothBuilder.SelfIntersectionCheckingOption CHECK
public static final TBSSmoothBuilder.SelfIntersectionCheckingOption RUNTIME
public static final TBSSmoothBuilder.SelfIntersectionCheckingOption ITERATIVE
public static final int _OFF
public static final int _CHECK
public static final int _RUNTIME
public static final int _ITERATIVE
public static TBSSmoothBuilder.SelfIntersectionCheckingOption valueOf(int value)
public static TBSSmoothBuilder.SelfIntersectionCheckingOption valueOf(String name)
public static TBSSmoothBuilder.SelfIntersectionCheckingOption[] values()
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.