Package | Description |
---|---|
nxopen.cae |
Provides classes and interfaces relating to Advanced Simulation and Design Simulation.
|
Modifier and Type | Field and Description |
---|---|
static WeldBuilder.WeldLocation |
WeldBuilder.WeldLocation.EDGE
Creates a weld at locations on an edge
|
static WeldBuilder.WeldLocation |
WeldBuilder.WeldLocation.FILE
Creates a weld at locations specified in an input file
|
static WeldBuilder.WeldLocation |
WeldBuilder.WeldLocation.NODE
Creates a weld at locations specified using nodes
|
static WeldBuilder.WeldLocation |
WeldBuilder.WeldLocation.POINT
Creates a weld at locations specified using points
|
Modifier and Type | Method and Description |
---|---|
WeldBuilder.WeldLocation |
WeldBuilder.location()
Returns the location of the specified weld
License requirements: None. |
static WeldBuilder.WeldLocation |
WeldBuilder.WeldLocation.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static WeldBuilder.WeldLocation |
WeldBuilder.WeldLocation.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static WeldBuilder.WeldLocation[] |
WeldBuilder.WeldLocation.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
WeldBuilder.setLocation(WeldBuilder.WeldLocation location)
License requirements: nx_masterfem ("Finite Element Modeling") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.