Package | Description |
---|---|
nxopen.cae |
Provides classes and interfaces relating to Advanced Simulation and Design Simulation.
|
Modifier and Type | Field and Description |
---|---|
static WeldBuilder.NumberOfPointsOnEdgeType |
WeldBuilder.NumberOfPointsOnEdgeType.MAXIMUM_NUMBER
Create the maximum number of points on an edge
|
static WeldBuilder.NumberOfPointsOnEdgeType |
WeldBuilder.NumberOfPointsOnEdgeType.SPECIFIED_NUMBER
Specify the number of points to be created on an edge
|
Modifier and Type | Method and Description |
---|---|
WeldBuilder.NumberOfPointsOnEdgeType |
WeldBuilder.numberOfPointsOption()
Returns the option to specify the maximum number of points on the edge(s) used to specify the location of the weld
License requirements: None. |
static WeldBuilder.NumberOfPointsOnEdgeType |
WeldBuilder.NumberOfPointsOnEdgeType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static WeldBuilder.NumberOfPointsOnEdgeType |
WeldBuilder.NumberOfPointsOnEdgeType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static WeldBuilder.NumberOfPointsOnEdgeType[] |
WeldBuilder.NumberOfPointsOnEdgeType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
WeldBuilder.setNumberOfPointsOption(WeldBuilder.NumberOfPointsOnEdgeType pointOnEdgeOption)
License requirements: nx_masterfem ("Finite Element Modeling") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.