Package | Description |
---|---|
nxopen.cae |
Provides classes and interfaces relating to Advanced Simulation and Design Simulation.
|
Modifier and Type | Field and Description |
---|---|
static SolverAppendOption.ImportBehaviorOption |
SolverAppendOption.ImportBehaviorOption.APPEND_MODEL |
static SolverAppendOption.ImportBehaviorOption |
SolverAppendOption.ImportBehaviorOption.MERGE_WITH_EXISTING |
Modifier and Type | Method and Description |
---|---|
SolverAppendOption.ImportBehaviorOption |
SolverAppendOption.importBehavior()
Returns the import behavior choice
License requirements: nx_masterfem ("Finite Element Modeling") OR nx_design_sim ("NX Design Simulation") . |
static SolverAppendOption.ImportBehaviorOption |
SolverAppendOption.ImportBehaviorOption.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static SolverAppendOption.ImportBehaviorOption |
SolverAppendOption.ImportBehaviorOption.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static SolverAppendOption.ImportBehaviorOption[] |
SolverAppendOption.ImportBehaviorOption.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
SolverAppendOption.setImportBehavior(SolverAppendOption.ImportBehaviorOption behaviorOption)
License requirements: nx_masterfem ("Finite Element Modeling") OR nx_design_sim ("NX Design Simulation") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.