Package | Description |
---|---|
nxopen.cae |
Provides classes and interfaces relating to Advanced Simulation and Design Simulation.
|
Modifier and Type | Field and Description |
---|---|
static SolidPropertyCheckBuilder.UserUnit |
SolidPropertyCheckBuilder.UserUnit.DEFAULT_UNIT
Load unit = same as system default unit
|
static SolidPropertyCheckBuilder.UserUnit |
SolidPropertyCheckBuilder.UserUnit.KG_MILLI
mass = kg, cg = mm, volume = mm^3 mmoi = kg-mm^2
|
static SolidPropertyCheckBuilder.UserUnit |
SolidPropertyCheckBuilder.UserUnit.LBF_IN_SEC
mass = lbf-sec^2/in, cg = in, volume = in^3 mmoi = lbf-in-sec^2
|
static SolidPropertyCheckBuilder.UserUnit |
SolidPropertyCheckBuilder.UserUnit.LBM_IN
mass = lbm, cg = in, volume = in^3 mmoi = lbm-in^2
|
Modifier and Type | Method and Description |
---|---|
SolidPropertyCheckBuilder.UserUnit |
SolidPropertyCheckBuilder.userSpecifiedUnit()
Returns the output result unit
License requirements: None. |
static SolidPropertyCheckBuilder.UserUnit |
SolidPropertyCheckBuilder.UserUnit.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static SolidPropertyCheckBuilder.UserUnit |
SolidPropertyCheckBuilder.UserUnit.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static SolidPropertyCheckBuilder.UserUnit[] |
SolidPropertyCheckBuilder.UserUnit.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
SolidPropertyCheckBuilder.setUserSpecifiedUnit(SolidPropertyCheckBuilder.UserUnit userSpecifiedUnit)
License requirements: nx_masterfem ("Finite Element Modeling") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.