Package | Description |
---|---|
nxopen.cae |
Provides classes and interfaces relating to Advanced Simulation and Design Simulation.
|
Modifier and Type | Field and Description |
---|---|
static SimSolution.SolveOption |
SimSolution.SolveOption.EDIT_SOLVER_INPUT_FILE
edit existing solver input file
|
static SimSolution.SolveOption |
SimSolution.SolveOption.SOLVE
write solver input file and launch solve
|
static SimSolution.SolveOption |
SimSolution.SolveOption.SOLVE_INPUT_FILE
launch solve with existing solver input file
|
static SimSolution.SolveOption |
SimSolution.SolveOption.WRITE_EDIT_AND_SOLVE_INPUT_FILE
write solver input file, allow edit and then launch solve
|
static SimSolution.SolveOption |
SimSolution.SolveOption.WRITE_SOLVER_INPUT_FILE
write solver input file only
|
Modifier and Type | Method and Description |
---|---|
static SimSolution.SolveOption |
SimSolution.SolveOption.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static SimSolution.SolveOption |
SimSolution.SolveOption.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static SimSolution.SolveOption[] |
SimSolution.SolveOption.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
SimSolution.solve(SimSolution.SolveOption solveOption,
SimSolution.SetupCheckOption setupCheckOption)
Solves the solution
License requirements: nx_masterfem ("Finite Element Modeling") OR nx_design_sim ("NX Design Simulation") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.