Package | Description |
---|---|
nxopen.cae |
Provides classes and interfaces relating to Advanced Simulation and Design Simulation.
|
Modifier and Type | Interface and Description |
---|---|
interface |
SimAutoBcRecipe
Represents a simulation recipe containing the parameters needed
for the generation of a set of face pairs from the faces/bodies in the model
To create a new instance of this class, use SimRecipeCollection.createAutoBcRecipe(java.lang.String, java.lang.String) Created in NX5.0.0 |
Modifier and Type | Method and Description |
---|---|
SimRecipe |
SimRecipeCollection.findObject(String journalIdentifier)
Finds the
SimRecipe with the given identifier as recorded in a journal. |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.