Package | Description |
---|---|
nxopen.cae |
Provides classes and interfaces relating to Advanced Simulation and Design Simulation.
|
Modifier and Type | Method and Description |
---|---|
SimLoad |
SimLoadCollection.createLoad(String descriptorName,
String name)
Creates a load for the load descriptor passed
License requirements: nx_masterfem ("Finite Element Modeling") OR nx_design_sim ("NX Design Simulation") . |
SimLoad |
SimLoadCollection.findObject(String journalIdentifier)
Finds the
SimLoad with the given identifier as recorded in a journal. |
SimLoad[] |
MechanicalLoadSumBuilder.getLoads()
The load objects
License requirements: None. |
SimLoad[] |
SimLoadSet.getMemberFolderValidLoads(SimLbcFolder tFolder)
Get all valid loads under given root folder in given load set
License requirements: nx_masterfem ("Finite Element Modeling") OR nx_design_sim ("NX Design Simulation") . |
SimLoad[] |
SimLoadSet.getMemberLoads()
Get all load memebers from load set
License requirements: nx_masterfem ("Finite Element Modeling") OR nx_design_sim ("NX Design Simulation") . |
Modifier and Type | Method and Description |
---|---|
void |
SimLoadSet.addMemberLoads(SimLoad[] tmembers)
Add load members to load set.
|
void |
SimLoadSet.removeMemberLoads(SimLoad[] tmembers)
Remove load memebers from load set
License requirements: nx_masterfem ("Finite Element Modeling") OR nx_design_sim ("NX Design Simulation") . |
void |
MechanicalLoadSumBuilder.setLoads(SimLoad[] loads)
Sets the loads
License requirements: nx_masterfem ("Finite Element Modeling") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.