Package | Description |
---|---|
nxopen.cae |
Provides classes and interfaces relating to Advanced Simulation and Design Simulation.
|
Modifier and Type | Field and Description |
---|---|
static SimBcXyPlotBuilder.ResolveMultipleMatches |
SimBcXyPlotBuilder.ResolveMultipleMatches.ADD |
static SimBcXyPlotBuilder.ResolveMultipleMatches |
SimBcXyPlotBuilder.ResolveMultipleMatches.AVERAGE |
static SimBcXyPlotBuilder.ResolveMultipleMatches |
SimBcXyPlotBuilder.ResolveMultipleMatches.MAXIMUM |
static SimBcXyPlotBuilder.ResolveMultipleMatches |
SimBcXyPlotBuilder.ResolveMultipleMatches.MINIMUM |
static SimBcXyPlotBuilder.ResolveMultipleMatches |
SimBcXyPlotBuilder.ResolveMultipleMatches.MULTIPLE_CURVES |
Modifier and Type | Method and Description |
---|---|
SimBcXyPlotBuilder.ResolveMultipleMatches |
SimBcXyPlotBuilder.multipleMatches()
Returns a
SimBcXyPlotBuilder.ResolveMultipleMatches used in plot to resolve multiple values
License requirements: nx_masterfem ("Finite Element Modeling") Created in NX9.0.0 |
static SimBcXyPlotBuilder.ResolveMultipleMatches |
SimBcXyPlotBuilder.ResolveMultipleMatches.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static SimBcXyPlotBuilder.ResolveMultipleMatches |
SimBcXyPlotBuilder.ResolveMultipleMatches.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static SimBcXyPlotBuilder.ResolveMultipleMatches[] |
SimBcXyPlotBuilder.ResolveMultipleMatches.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
SimBcXyPlotBuilder.setMultipleMatches(SimBcXyPlotBuilder.ResolveMultipleMatches resolveMultipleMatches)
License requirements: nx_masterfem ("Finite Element Modeling") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.