Package | Description |
---|---|
nxopen.cae |
Provides classes and interfaces relating to Advanced Simulation and Design Simulation.
|
Modifier and Type | Field and Description |
---|---|
static SimBcPlotContoursBuilder.ResolveOverlapType |
SimBcPlotContoursBuilder.ResolveOverlapType.ADD |
static SimBcPlotContoursBuilder.ResolveOverlapType |
SimBcPlotContoursBuilder.ResolveOverlapType.AVERAGE |
static SimBcPlotContoursBuilder.ResolveOverlapType |
SimBcPlotContoursBuilder.ResolveOverlapType.MAXIMUM |
static SimBcPlotContoursBuilder.ResolveOverlapType |
SimBcPlotContoursBuilder.ResolveOverlapType.MINIMUM |
static SimBcPlotContoursBuilder.ResolveOverlapType |
SimBcPlotContoursBuilder.ResolveOverlapType.SPECIFY |
Modifier and Type | Method and Description |
---|---|
SimBcPlotContoursBuilder.ResolveOverlapType |
SimBcPlotContoursBuilder.resolveOverlap()
Returns a
SimBcPlotContoursBuilder.ResolveOverlapType used in plot to resolve overlapping values
License requirements: nx_masterfem ("Finite Element Modeling") Created in NX8.5.0 |
static SimBcPlotContoursBuilder.ResolveOverlapType |
SimBcPlotContoursBuilder.ResolveOverlapType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static SimBcPlotContoursBuilder.ResolveOverlapType |
SimBcPlotContoursBuilder.ResolveOverlapType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static SimBcPlotContoursBuilder.ResolveOverlapType[] |
SimBcPlotContoursBuilder.ResolveOverlapType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
SimBcPlotContoursBuilder.setResolveOverlap(SimBcPlotContoursBuilder.ResolveOverlapType resolveOverlapType)
License requirements: nx_masterfem ("Finite Element Modeling") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.