Package | Description |
---|---|
nxopen.cae |
Provides classes and interfaces relating to Advanced Simulation and Design Simulation.
|
Modifier and Type | Field and Description |
---|---|
static ResultsManipulationBuilder.ElementValueAtNode |
ResultsManipulationBuilder.ElementValueAtNode.AVERAGE |
static ResultsManipulationBuilder.ElementValueAtNode |
ResultsManipulationBuilder.ElementValueAtNode.MAXIMUM |
static ResultsManipulationBuilder.ElementValueAtNode |
ResultsManipulationBuilder.ElementValueAtNode.MINIMUM |
static ResultsManipulationBuilder.ElementValueAtNode |
ResultsManipulationBuilder.ElementValueAtNode.SUM |
Modifier and Type | Method and Description |
---|---|
static ResultsManipulationBuilder.ElementValueAtNode |
ResultsManipulationBuilder.ElementValueAtNode.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static ResultsManipulationBuilder.ElementValueAtNode |
ResultsManipulationBuilder.ElementValueAtNode.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static ResultsManipulationBuilder.ElementValueAtNode[] |
ResultsManipulationBuilder.ElementValueAtNode.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
ResultsReductionBuilder.setElementValueAtNode(ResultsManipulationBuilder.ElementValueAtNode value)
Set element value to be used at a node
License requirements: nx_masterfem ("Finite Element Modeling") OR nx_design_sim ("NX Design Simulation") . |
void |
ResultsEnvelopeBuilder.setElementValueAtNode(ResultsManipulationBuilder.ElementValueAtNode value)
Set element value to be used at a node
License requirements: nx_masterfem ("Finite Element Modeling") OR nx_design_sim ("NX Design Simulation") . |
void |
ResultsCombinationBuilder.setElementValueAtNode(ResultsManipulationBuilder.ElementValueAtNode value)
Set element value to be used at a node
License requirements: nx_masterfem ("Finite Element Modeling") OR nx_design_sim ("NX Design Simulation") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.