Package | Description |
---|---|
nxopen.cae |
Provides classes and interfaces relating to Advanced Simulation and Design Simulation.
|
Modifier and Type | Field and Description |
---|---|
ResultParameters |
Post.ResultForPostviewData.resultParamter
a copy of the
ResultParameters which defines input postview, It is user's responsibility to destroy the result parameters object once done
using ResultManager.deleteResultParameters(nxopen.cae.ResultParameters) , in order to free up system resources |
Modifier and Type | Method and Description |
---|---|
ResultParameters |
ResultManager.createResultParameters()
Creates a result parameter object.
|
ResultParameters |
CrossSectionParameters.getModelRangeParameters()
Ask model range parameters
License requirements: nx_masterfem ("Finite Element Modeling") OR nx_design_sim ("NX Design Simulation") . |
ResultParameters |
ResultAccess.getParameters()
Returns the
ResultParameters which defines the current result state. |
Modifier and Type | Method and Description |
---|---|
PostGraphAcrossIterationsBuilder |
ResultManager.createGraphAcrossIterationsBuilder(Result result,
ResultParameters parameter)
Returns a builder used for creating graphs across iterations of result values of result parameter.
|
PostGraphAcrossIterationsBuilder |
ResultManager.createGraphAcrossIterationsBuilder(Result result,
ResultParameters[] parameters,
String[] names,
String formula)
Returns a builder used for creating graphs across iterations of result values of expression.
|
PostGraphAcrossIterationsBuilder |
ResultManager.createGraphAcrossIterationsBuilder(Result result,
ResultParameters parameter1,
ResultParameters parameter2)
Returns a builder used for creating graphs across iterations of result values two result parameters.
|
PostGraphAlongPathBuilder |
ResultManager.createGraphAlongPathBuilder(Result result,
ResultParameters parameter)
Returns a builder used for creating the graph of result values series of entities
or path object defined by result parameter.
|
PostGraphAlongPathBuilder |
ResultManager.createGraphAlongPathBuilder(Result result,
ResultParameters parameter1,
ResultParameters parameter2)
Returns a builder used for creating the graph of result values of series of entities
or path object defined by two result parameter.
|
PostGraphOrbitBuilder |
ResultManager.createGraphOrbitBuilder(Result result,
ResultParameters parameter)
Returns a builder used for creating the orbit graph from result defined by result parameter.
|
int |
Post.createPostviewForResult(int viewIndex,
Result result,
boolean overlay,
ResultParameters resultParamter)
Create a new post view with specified result on a loaded result id.
|
int[] |
Post.createPostviewsForResultAndSE(int viewIndex,
Result result,
ResultParameters resultParamter)
Create a new post view with specified result on a loaded result id.
|
ResultAccess |
ResultManager.createResultAccess(Result result,
ResultParameters parameters)
Creates a result access object
It is user's responsibility to destroy the result access object once done
using
ResultManager.deleteResultAccess(nxopen.cae.ResultAccess) , in order to free up system resources
License requirements: nx_masterfem ("Finite Element Modeling") OR nx_design_sim ("NX Design Simulation") Created in NX6.0.2 |
FieldReference |
ResultManager.createResultAccessReferenceField(FieldManager fieldManager,
Result result,
ResultParameters parameters,
String depDemainName,
String fieldName)
Creates a result access reference field object.
|
void |
ResultManager.deleteResultParameters(ResultParameters result)
Delete a
ResultParameters object. |
void |
Post.postviewSetResult(int postviewId,
ResultParameters resultParamter)
Set the result for color display in the input postview id.
|
void |
CreateJtBuilder.setExportData(ResultParameters[] parameters,
int[] templateIds,
CreateJtBuilder.Component[] componentToExport)
The result parameters
License requirements: nx_masterfem ("Finite Element Modeling") OR nx_design_sim ("NX Design Simulation") . |
void |
ResultAccess.setParameters(ResultParameters resultParameters)
Sets
ResultParameters . |
void |
TransientResultsReductionBuilder.setResult(Result result,
ResultParameters[] parameters,
String[] names)
The result types
License requirements: nx_masterfem ("Finite Element Modeling") OR nx_design_sim ("NX Design Simulation") . |
void |
ResultsEnvelopeBuilder.setResults(int[] ids,
Result[] results,
ResultParameters[] parameters)
The results
License requirements: nx_masterfem ("Finite Element Modeling") OR nx_design_sim ("NX Design Simulation") . |
void |
ResultsEnvelopeBuilder.setResults(Result[] results,
ResultParameters[] parameters)
The results
License requirements: nx_masterfem ("Finite Element Modeling") OR nx_design_sim ("NX Design Simulation") . |
void |
ResultsReductionBuilder.setResults(Result[] results,
ResultParameters[] parameters,
String[] names)
The result types
License requirements: nx_masterfem ("Finite Element Modeling") OR nx_design_sim ("NX Design Simulation") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.