Package | Description |
---|---|
nxopen.cae |
Provides classes and interfaces relating to Advanced Simulation and Design Simulation.
|
Modifier and Type | Field and Description |
---|---|
Result.Type |
Result.ResultParameters.type
Deprecated.
|
Result.Type |
Result.DeformationParameters.type
Deprecated.
|
Result.Type |
Result.VelocityParameters.type |
Result.Type[] |
Result.AskResultTypesData.types |
Modifier and Type | Method and Description |
---|---|
Result.Type |
ResultParameters.getResultType()
Deprecated.
Deprecated in NX8.0.0. Use
ResultParameters.getGenericResultType() instead.
|
Modifier and Type | Method and Description |
---|---|
Result.DataType |
Result.askResultDataType(int loadcaseIndex,
int iterationIndex,
Result.Type resultType)
Ask result datatype
License requirements: nx_masterfem ("Finite Element Modeling") OR nx_design_sim ("NX Design Simulation") . |
int[] |
Result.askResultSections(int loadcaseIndex,
int iterationIndex,
Result.Type resultType)
Ask element ids and corresponding number of sections at which result is defined
License requirements: nx_masterfem ("Finite Element Modeling") OR nx_design_sim ("NX Design Simulation") . |
ResultMeasure |
ResultMeasureCollection.createResultMeasure(SimSolution tSol,
int iStepIndex,
int iIterIndex,
Result.Type pType,
Result.Component eComp,
String expName)
Deprecated.
Deprecated in NX10.0.0. Use
ResultMeasureCollection.createResultMeasureNew(nxopen.cae.ResultMeasureResultOptions, nxopen.cae.ResultMeasureModelSubset, java.lang.String) instead.
|
ResultMeasureResultOptions |
ResultMeasureCollection.createResultOptions(SimSolution tSol,
int iStepIndex,
int iIterIndex,
Result.Type pType,
Result.Component eComp)
Deprecated.
|
ResultMeasureResultOptions |
ResultMeasureCollection.createResultOptionsNew(SimSolution tSol,
SimResultReference tResultReference,
int iStepIndex,
int iIterIndex,
Result.Type pType,
Result.Component eComp)
Create a result options for result measure
License requirements: nx_masterfem ("Finite Element Modeling") . |
boolean |
Result.isResultTypeComplex(int loadcaseIndex,
int iterationIndex,
Result.Type resultType)
Ask whether a result type is complex or not
License requirements: nx_masterfem ("Finite Element Modeling") OR nx_design_sim ("NX Design Simulation") . |
void |
ResultParameters.setResultType(Result.Type type)
Deprecated.
Deprecated in NX8.0.0. Use
ResultParameters.getGenericResultType() instead.
|
Constructor and Description |
---|
DeformationParameters(int loadCaseIndexInitial,
int iterationIndexInitial,
Result.Type typeInitial,
Result.Complex complexInitial,
double phaseAngleInitial,
Result.DeformationScale deformationScaleInitial,
double absoluteScaleValueInitial,
double modelPercentScaleValueInitial)
Deprecated.
Constructor for the DeformationParameters object.
|
ResultParameters(int loadCaseIndexInitial,
int iterationIndexInitial,
Result.Type typeInitial,
Result.Component componentInitial,
Result.ResultSection resSectionInitial,
int sectionInitial,
int plynumberInitial,
int layerInitial,
Result.Averaging averagingInitial,
boolean includeMidnodeInitial,
Result.CoordinateSystem coordinateSystemInitial,
boolean displayBeamResultInLocalCsysInitial,
Result.ElementValue elementValueInitial,
Result.Complex complexInitial,
double phaseAngleInitial,
boolean absoluteValueInitial,
double scaleValueInitial,
Unit unitInitial,
boolean calculateBeamStrResultsInitial,
boolean addBeamStrFilletsInitial,
double beamFilletRadiusInitial)
Deprecated.
Constructor for the ResultParameters object.
|
VelocityParameters(int loadCaseIndexInitial,
int iterationIndexInitial,
Result.Type typeInitial)
Constructor for the VelocityParameters object.
|
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.