Package | Description |
---|---|
nxopen.cae |
Provides classes and interfaces relating to Advanced Simulation and Design Simulation.
|
Modifier and Type | Field and Description |
---|---|
static Result.TensorDerivedAbsolute |
Result.TensorDerivedAbsolute.ALL_COMPONENTS
Absolute of primary components first
|
static Result.TensorDerivedAbsolute |
Result.TensorDerivedAbsolute.DERIVED_COMPONENT
Absolute of current derived components
|
Modifier and Type | Method and Description |
---|---|
Result.TensorDerivedAbsolute |
ResultParameters.getTensorComponentAbsoluteValue()
Get the method used when calculating the absolute values for the derived components of
CAE.Result.DataType#TENSOR like CAE.Result.Component#MAXIMUM_PRINCIPAL
License requirements: nx_masterfem ("Finite Element Modeling") OR nx_design_sim ("NX Design Simulation") Created in NX8.0.1 |
Result.TensorDerivedAbsolute |
CrossSectionParameters.getTensorComponentAbsoluteValue()
Get the method used when calculating the absolute values for the derived components of
nxopen.cae.Result.DataType.Tensor like nxopen.cae.Result.Component.MaximumPrincipal
License requirements: nx_masterfem ("Finite Element Modeling") OR nx_design_sim ("NX Design Simulation") Created in NX8.0.1 |
static Result.TensorDerivedAbsolute |
Result.TensorDerivedAbsolute.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static Result.TensorDerivedAbsolute |
Result.TensorDerivedAbsolute.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static Result.TensorDerivedAbsolute[] |
Result.TensorDerivedAbsolute.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
ResultParameters.setTensorComponentAbsoluteValue(Result.TensorDerivedAbsolute absolute)
Set the method used when calculating the absolute values for the derived components of
CAE.Result.DataType#TENSOR
like CAE.Result.Component#MAXIMUM_PRINCIPAL
License requirements: nx_masterfem ("Finite Element Modeling") OR nx_design_sim ("NX Design Simulation") Created in NX8.0.1 |
void |
CrossSectionParameters.setTensorComponentAbsoluteValue(Result.TensorDerivedAbsolute absolute)
Set the method used when calculating the absolute values for the derived components of
nxopen.cae.Result.DataType.Tensor
like nxopen.cae.Result.Component.MaximumPrincipal
License requirements: nx_masterfem ("Finite Element Modeling") OR nx_design_sim ("NX Design Simulation") Created in NX8.0.1 |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.