Package | Description |
---|---|
nxopen.cae |
Provides classes and interfaces relating to Advanced Simulation and Design Simulation.
|
Modifier and Type | Field and Description |
---|---|
static Result.CoordinateSystemSource |
Result.CoordinateSystemSource.MODEL
identifies a coordinate system in the work part
|
static Result.CoordinateSystemSource |
Result.CoordinateSystemSource.NONE |
static Result.CoordinateSystemSource |
Result.CoordinateSystemSource.RESULT
identifies a coordinate system in the result
|
Result.CoordinateSystemSource |
ResultParameters.SelectedCoordinateSystemData.source |
Result.CoordinateSystemSource |
ClippingParameters.SelectedCoordinateSystemData.source |
Modifier and Type | Method and Description |
---|---|
Result.CoordinateSystemSource |
FreeBodyResultsBuilder.getLocationCsysSource()
The source for the location coordinate system
License requirements: nx_masterfem ("Finite Element Modeling") OR nx_design_sim ("NX Design Simulation") . |
Result.CoordinateSystemSource |
FreeBodyResultsBuilder.getSelectedReferenceCsysSource()
The source for the selected reference coordinate system
License requirements: nx_masterfem ("Finite Element Modeling") OR nx_design_sim ("NX Design Simulation") . |
static Result.CoordinateSystemSource |
Result.CoordinateSystemSource.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static Result.CoordinateSystemSource |
Result.CoordinateSystemSource.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static Result.CoordinateSystemSource[] |
Result.CoordinateSystemSource.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
FreeBodyResultsBuilder.setLocationCsysSource(Result.CoordinateSystemSource source)
The source for the location coordinate system
License requirements: nx_masterfem ("Finite Element Modeling") OR nx_design_sim ("NX Design Simulation") . |
void |
ResultParameters.setSelectedCoordinateSystem(Result.CoordinateSystemSource source,
int id)
Set selected coordinate system in which results are to be presented
Coordinate systems labels defined in a result file can be retrieved using
CAE.Result#getResultCoordinateSystems
License requirements: nx_masterfem ("Finite Element Modeling") OR nx_design_sim ("NX Design Simulation") Created in NX7.5.1 |
void |
ClippingParameters.setSelectedCoordinateSystem(Result.CoordinateSystemSource source,
int id)
Set selected coordinate system
License requirements: nx_masterfem ("Finite Element Modeling") OR nx_design_sim ("NX Design Simulation") . |
void |
FreeBodyResultsBuilder.setSelectedReferenceCsysSource(Result.CoordinateSystemSource source)
The source for the selected reference coordinate system
License requirements: nx_masterfem ("Finite Element Modeling") OR nx_design_sim ("NX Design Simulation") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.