Package | Description |
---|---|
nxopen.cae |
Provides classes and interfaces relating to Advanced Simulation and Design Simulation.
|
Modifier and Type | Field and Description |
---|---|
static Result.CoordinateSystem |
Result.CoordinateSystem.ABSOLUTE_CYLINDRICAL |
static Result.CoordinateSystem |
Result.CoordinateSystem.ABSOLUTE_RECTANGULAR |
static Result.CoordinateSystem |
Result.CoordinateSystem.ABSOLUTE_SPHERICAL |
Result.CoordinateSystem |
Result.ResultParameters.coordinateSystem
Deprecated.
|
static Result.CoordinateSystem |
Result.CoordinateSystem.LOCAL |
static Result.CoordinateSystem |
Result.CoordinateSystem.MATERIAL
Material coordinate system is applicable only when
such coordinate systems are defined in the results model;
if no material coordinate system is defined
ABSOLUTE_RECTANGULAR
will be used |
Result.CoordinateSystem |
Post.Clipping.planeCoordinateSystem
Any absolute or work
|
static Result.CoordinateSystem |
Result.CoordinateSystem.SELECT_CYLINDRICAL |
static Result.CoordinateSystem |
Result.CoordinateSystem.SELECT_RECTANGULAR |
static Result.CoordinateSystem |
Result.CoordinateSystem.SELECT_SPHERICAL |
Result.CoordinateSystem |
Result.ResultCoordinateSystemDefinitionData.type
|
static Result.CoordinateSystem |
Result.CoordinateSystem.WORK_CYLINDRICAL |
static Result.CoordinateSystem |
Result.CoordinateSystem.WORK_RECTANGULAR |
static Result.CoordinateSystem |
Result.CoordinateSystem.WORK_SPHERICAL |
Modifier and Type | Method and Description |
---|---|
Result.CoordinateSystem |
ResultVariable.csys()
Returns the Co-ordinate System
License requirements: nx_masterfem ("Finite Element Modeling") OR nx_design_sim ("NX Design Simulation") . |
Result.CoordinateSystem |
ResultParameters.getCoordinateSystem()
Ask result coordinate system
License requirements: nx_masterfem ("Finite Element Modeling") OR nx_design_sim ("NX Design Simulation") . |
Result.CoordinateSystem |
ClippingParameters.getCoordinateSystem()
Ask coordinate system
License requirements: nx_masterfem ("Finite Element Modeling") OR nx_design_sim ("NX Design Simulation") . |
Result.CoordinateSystem |
FreeBodyResultsBuilder.getReferenceCsys()
The reference coordinate system
License requirements: nx_masterfem ("Finite Element Modeling") OR nx_design_sim ("NX Design Simulation") . |
static Result.CoordinateSystem |
Result.CoordinateSystem.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static Result.CoordinateSystem |
Result.CoordinateSystem.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static Result.CoordinateSystem[] |
Result.CoordinateSystem.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
ResultParameters.setCoordinateSystem(Result.CoordinateSystem coordinate)
Set result coordinate system
License requirements: nx_masterfem ("Finite Element Modeling") OR nx_design_sim ("NX Design Simulation") . |
void |
ResultMeasureResultDirectionSectionOptions.setCoordinateSystem(Result.CoordinateSystem eCsys)
Set the coordinate system for directional components
License requirements: nx_masterfem ("Finite Element Modeling") OR nx_design_sim ("NX Design Simulation") . |
void |
ResultMeasureResultDirectionOptions.setCoordinateSystem(Result.CoordinateSystem eCsys)
Set the coordinate system for directional components
License requirements: nx_masterfem ("Finite Element Modeling") OR nx_design_sim ("NX Design Simulation") . |
void |
ResultMeasureResultAllOptions.setCoordinateSystem(Result.CoordinateSystem eCsys)
Set the coordinate system for directional components
License requirements: nx_masterfem ("Finite Element Modeling") OR nx_design_sim ("NX Design Simulation") . |
void |
ClippingParameters.setCoordinateSystem(Result.CoordinateSystem coordinateSystem)
Set coordinate system
License requirements: nx_masterfem ("Finite Element Modeling") OR nx_design_sim ("NX Design Simulation") . |
void |
ResultVariable.setCsys(Result.CoordinateSystem csys)
License requirements: nx_masterfem ("Finite Element Modeling") OR nx_design_sim ("NX Design Simulation") . |
void |
FreeBodyResultsBuilder.setReferenceCsys(Result.CoordinateSystem csys)
The reference coordinate system
License requirements: nx_masterfem ("Finite Element Modeling") OR nx_design_sim ("NX Design Simulation") . |
Constructor and Description |
---|
Clipping(boolean showOutlineInitial,
boolean showClippedGhostInitial,
double clipValueInitial,
Post.ClipSide sideInitial,
Post.ClipPlane planeInitial,
Result.CoordinateSystem planeCoordinateSystemInitial)
Constructor for the Clipping object.
|
ResultParameters(int loadCaseIndexInitial,
int iterationIndexInitial,
Result.Type typeInitial,
Result.Component componentInitial,
Result.ResultSection resSectionInitial,
int sectionInitial,
int plynumberInitial,
int layerInitial,
Result.Averaging averagingInitial,
boolean includeMidnodeInitial,
Result.CoordinateSystem coordinateSystemInitial,
boolean displayBeamResultInLocalCsysInitial,
Result.ElementValue elementValueInitial,
Result.Complex complexInitial,
double phaseAngleInitial,
boolean absoluteValueInitial,
double scaleValueInitial,
Unit unitInitial,
boolean calculateBeamStrResultsInitial,
boolean addBeamStrFilletsInitial,
double beamFilletRadiusInitial)
Deprecated.
Constructor for the ResultParameters object.
|
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.