Package | Description |
---|---|
nxopen.cae |
Provides classes and interfaces relating to Advanced Simulation and Design Simulation.
|
Modifier and Type | Field and Description |
---|---|
static Result.Component |
Result.Component.AXIAL |
static Result.Component |
Result.Component.BENDING_S |
static Result.Component |
Result.Component.BENDING_T |
static Result.Component |
Result.Component.BENDING_XX |
static Result.Component |
Result.Component.BENDING_XY |
static Result.Component |
Result.Component.BENDING_YY |
Result.Component |
Result.ResultParameters.component
Deprecated.
|
Result.Component[] |
ResultAccess.AskResultComponentsData.components |
Result.Component[] |
BaseResultType.AskComponentsData.components |
static Result.Component |
Result.Component.DETERMINANT |
static Result.Component |
Result.Component.MAGNITUDE |
static Result.Component |
Result.Component.MAXIMUM_PRINCIPAL |
static Result.Component |
Result.Component.MAXIMUM_SHEAR |
static Result.Component |
Result.Component.MEAN |
static Result.Component |
Result.Component.MEMBRANE_XX |
static Result.Component |
Result.Component.MEMBRANE_XY |
static Result.Component |
Result.Component.MEMBRANE_YY |
static Result.Component |
Result.Component.MIDDLE_PRINCIPAL |
static Result.Component |
Result.Component.MINIMUM_PRINCIPAL |
static Result.Component |
Result.Component.OCTAHEDRAL |
static Result.Component |
Result.Component.SCALAR |
static Result.Component |
Result.Component.SCALAR1 |
static Result.Component |
Result.Component.SCALAR2 |
static Result.Component |
Result.Component.SCALAR3 |
static Result.Component |
Result.Component.SCALAR4 |
static Result.Component |
Result.Component.SCALAR5 |
static Result.Component |
Result.Component.SCALAR6 |
static Result.Component |
Result.Component.SHEAR_S |
static Result.Component |
Result.Component.SHEAR_T |
static Result.Component |
Result.Component.SHEAR_XZ |
static Result.Component |
Result.Component.SHEAR_YZ |
static Result.Component |
Result.Component.SPRING_DASHPOT_FORCE
No longer used; it means
SPRING_DASHPOT_FORCE_X in new format |
static Result.Component |
Result.Component.SPRING_DASHPOT_FORCE_X |
static Result.Component |
Result.Component.SPRING_DASHPOT_FORCE_Y |
static Result.Component |
Result.Component.SPRING_DASHPOT_FORCE_Z |
static Result.Component |
Result.Component.SPRING_DASHPOT_MOMENT_X |
static Result.Component |
Result.Component.SPRING_DASHPOT_MOMENT_Y |
static Result.Component |
Result.Component.SPRING_DASHPOT_MOMENT_Z |
static Result.Component |
Result.Component.TORSION |
static Result.Component |
Result.Component.VON_MISES |
static Result.Component |
Result.Component.WORST_PRINCIPAL |
static Result.Component |
Result.Component.X |
static Result.Component |
Result.Component.XX |
static Result.Component |
Result.Component.XY |
static Result.Component |
Result.Component.Y |
static Result.Component |
Result.Component.YY |
static Result.Component |
Result.Component.YZ |
static Result.Component |
Result.Component.Z |
static Result.Component |
Result.Component.ZX |
static Result.Component |
Result.Component.ZZ |
Modifier and Type | Method and Description |
---|---|
Result.Component |
ResultVariable.comp()
Returns the Component
License requirements: nx_masterfem ("Finite Element Modeling") OR nx_design_sim ("NX Design Simulation") . |
Result.Component |
DeformationParameters.component()
Returns the result component that is used for deforming the model.
|
Result.Component |
ResultParameters.getResultComponent()
Ask result component
License requirements: nx_masterfem ("Finite Element Modeling") OR nx_design_sim ("NX Design Simulation") . |
Result.Component |
CrossSectionParameters.getResultComponent()
Ask result component
License requirements: nx_masterfem ("Finite Element Modeling") OR nx_design_sim ("NX Design Simulation") . |
static Result.Component |
Result.Component.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static Result.Component |
Result.Component.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static Result.Component[] |
Result.Component.values()
Returns an array that contains the values for this enum.
|
Result.Component |
PostGraphOrbitBuilder.xresultComponent()
Returns the component used as x axis for orbit plot
License requirements: nx_masterfem ("Finite Element Modeling") OR nx_design_sim ("NX Design Simulation") . |
Result.Component |
PostGraphOrbitBuilder.yresultComponent()
Returns the component used as y axis for orbit plot
License requirements: nx_masterfem ("Finite Element Modeling") OR nx_design_sim ("NX Design Simulation") . |
Modifier and Type | Method and Description |
---|---|
ResultMeasure |
ResultMeasureCollection.createResultMeasure(SimSolution tSol,
int iStepIndex,
int iIterIndex,
Result.Type pType,
Result.Component eComp,
String expName)
Deprecated.
Deprecated in NX10.0.0. Use
ResultMeasureCollection.createResultMeasureNew(nxopen.cae.ResultMeasureResultOptions, nxopen.cae.ResultMeasureModelSubset, java.lang.String) instead.
|
ResultMeasureResultOptions |
ResultMeasureCollection.createResultOptions(SimSolution tSol,
int iStepIndex,
int iIterIndex,
Result.Type pType,
Result.Component eComp)
Deprecated.
|
ResultMeasureResultOptions |
ResultMeasureCollection.createResultOptionsNew(SimSolution tSol,
SimResultReference tResultReference,
int iStepIndex,
int iIterIndex,
Result.Type pType,
Result.Component eComp)
Create a result options for result measure
License requirements: nx_masterfem ("Finite Element Modeling") . |
ResultVariable |
ResultManager.createResultvariable(SimSimulation sim,
Result.Quantity quan,
Result.Location loc,
Result.Component comp,
String restypename,
String name)
Creates Result Variable object
License requirements: nx_masterfem ("Finite Element Modeling") OR nx_design_sim ("NX Design Simulation") . |
void |
ResultVariable.setComp(Result.Component loc)
License requirements: nx_masterfem ("Finite Element Modeling") OR nx_design_sim ("NX Design Simulation") . |
void |
DeformationParameters.setComponent(Result.Component component)
License requirements: nx_masterfem ("Finite Element Modeling") OR nx_design_sim ("NX Design Simulation") . |
void |
ResultParameters.setResultComponent(Result.Component component)
Set result component
License requirements: nx_masterfem ("Finite Element Modeling") OR nx_design_sim ("NX Design Simulation") . |
void |
CrossSectionParameters.setResultComponent(Result.Component component)
Set result component
License requirements: nx_masterfem ("Finite Element Modeling") OR nx_design_sim ("NX Design Simulation") . |
void |
PostGraphOrbitBuilder.setXresultComponent(Result.Component xresult)
License requirements: nx_masterfem ("Finite Element Modeling") OR nx_design_sim ("NX Design Simulation") . |
void |
PostGraphOrbitBuilder.setYresultComponent(Result.Component yresult)
License requirements: nx_masterfem ("Finite Element Modeling") OR nx_design_sim ("NX Design Simulation") . |
Constructor and Description |
---|
ResultParameters(int loadCaseIndexInitial,
int iterationIndexInitial,
Result.Type typeInitial,
Result.Component componentInitial,
Result.ResultSection resSectionInitial,
int sectionInitial,
int plynumberInitial,
int layerInitial,
Result.Averaging averagingInitial,
boolean includeMidnodeInitial,
Result.CoordinateSystem coordinateSystemInitial,
boolean displayBeamResultInLocalCsysInitial,
Result.ElementValue elementValueInitial,
Result.Complex complexInitial,
double phaseAngleInitial,
boolean absoluteValueInitial,
double scaleValueInitial,
Unit unitInitial,
boolean calculateBeamStrResultsInitial,
boolean addBeamStrFilletsInitial,
double beamFilletRadiusInitial)
Deprecated.
Constructor for the ResultParameters object.
|
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.