Package | Description |
---|---|
nxopen.cae |
Provides classes and interfaces relating to Advanced Simulation and Design Simulation.
|
Modifier and Type | Field and Description |
---|---|
static Result.Complex |
Result.Complex.AMPLITUDE |
Result.Complex |
Result.ResultParameters.complex
Deprecated.
|
Result.Complex |
Result.DeformationParameters.complex
Deprecated.
|
static Result.Complex |
Result.Complex.IMAGINARY |
static Result.Complex |
Result.Complex.PHASE_ANGLE |
static Result.Complex |
Result.Complex.REAL |
static Result.Complex |
Result.Complex.SIGNED_AMPLITUDE |
Modifier and Type | Method and Description |
---|---|
Result.Complex |
ResultVariable.complex()
Returns the Complex type
License requirements: nx_masterfem ("Finite Element Modeling") OR nx_design_sim ("NX Design Simulation") . |
Result.Complex |
DeformationParameters.complexCriterion()
Returns the complexity criterion.
|
Result.Complex |
ResultParameters.getComplexCriterion()
If result is complex it returns which component is set(like real or imaginary)
License requirements: nx_masterfem ("Finite Element Modeling") OR nx_design_sim ("NX Design Simulation") . |
Result.Complex |
CrossSectionParameters.getComplexCriterion()
If result is complex it returns which component is set(like real or imaginary)
License requirements: nx_masterfem ("Finite Element Modeling") OR nx_design_sim ("NX Design Simulation") . |
static Result.Complex |
Result.Complex.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static Result.Complex |
Result.Complex.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static Result.Complex[] |
Result.Complex.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
ResultVariable.setComplex(Result.Complex complex)
License requirements: nx_masterfem ("Finite Element Modeling") OR nx_design_sim ("NX Design Simulation") . |
void |
ResultParameters.setComplexCriterion(Result.Complex complex)
Set complex criteria
License requirements: nx_masterfem ("Finite Element Modeling") OR nx_design_sim ("NX Design Simulation") . |
void |
DeformationParameters.setComplexCriterion(Result.Complex complex)
License requirements: nx_masterfem ("Finite Element Modeling") OR nx_design_sim ("NX Design Simulation") . |
void |
CrossSectionParameters.setComplexCriterion(Result.Complex complex)
Set complex criteria
License requirements: nx_masterfem ("Finite Element Modeling") OR nx_design_sim ("NX Design Simulation") . |
Constructor and Description |
---|
DeformationParameters(int loadCaseIndexInitial,
int iterationIndexInitial,
Result.Type typeInitial,
Result.Complex complexInitial,
double phaseAngleInitial,
Result.DeformationScale deformationScaleInitial,
double absoluteScaleValueInitial,
double modelPercentScaleValueInitial)
Deprecated.
Constructor for the DeformationParameters object.
|
ResultParameters(int loadCaseIndexInitial,
int iterationIndexInitial,
Result.Type typeInitial,
Result.Component componentInitial,
Result.ResultSection resSectionInitial,
int sectionInitial,
int plynumberInitial,
int layerInitial,
Result.Averaging averagingInitial,
boolean includeMidnodeInitial,
Result.CoordinateSystem coordinateSystemInitial,
boolean displayBeamResultInLocalCsysInitial,
Result.ElementValue elementValueInitial,
Result.Complex complexInitial,
double phaseAngleInitial,
boolean absoluteValueInitial,
double scaleValueInitial,
Unit unitInitial,
boolean calculateBeamStrResultsInitial,
boolean addBeamStrFilletsInitial,
double beamFilletRadiusInitial)
Deprecated.
Constructor for the ResultParameters object.
|
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.