Package | Description |
---|---|
nxopen.cae |
Provides classes and interfaces relating to Advanced Simulation and Design Simulation.
|
Modifier and Type | Field and Description |
---|---|
static ProjectNodesToCadGeometryBuilder.Operation |
ProjectNodesToCadGeometryBuilder.Operation.ADJUST
Adjust nodes that are off the geometry by more than the input tolerance by projecting them on to the CAD geometry
|
static ProjectNodesToCadGeometryBuilder.Operation |
ProjectNodesToCadGeometryBuilder.Operation.SHOW
Display information on nodes that are off the CAD geometry by more than the input tolerance
|
Modifier and Type | Method and Description |
---|---|
ProjectNodesToCadGeometryBuilder.Operation |
ProjectNodesToCadGeometryBuilder.operationState()
Returns the operation to be performed.
|
static ProjectNodesToCadGeometryBuilder.Operation |
ProjectNodesToCadGeometryBuilder.Operation.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static ProjectNodesToCadGeometryBuilder.Operation |
ProjectNodesToCadGeometryBuilder.Operation.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static ProjectNodesToCadGeometryBuilder.Operation[] |
ProjectNodesToCadGeometryBuilder.Operation.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
ProjectNodesToCadGeometryBuilder.setOperationState(ProjectNodesToCadGeometryBuilder.Operation operation)
License requirements: nx_masterfem ("Finite Element Modeling") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.