Package | Description |
---|---|
nxopen.cae |
Provides classes and interfaces relating to Advanced Simulation and Design Simulation.
|
Modifier and Type | Field and Description |
---|---|
static PostGraphBuilder.NodalCombination |
PostGraphBuilder.NodalCombination.AVERAGE |
static PostGraphBuilder.NodalCombination |
PostGraphBuilder.NodalCombination.MAXIMUM |
static PostGraphBuilder.NodalCombination |
PostGraphBuilder.NodalCombination.MINIMUM |
static PostGraphBuilder.NodalCombination |
PostGraphBuilder.NodalCombination.NONE |
static PostGraphBuilder.NodalCombination |
PostGraphBuilder.NodalCombination.SUM |
Modifier and Type | Method and Description |
---|---|
PostGraphBuilder.NodalCombination |
PostGraphBuilder.nodalCombinationValue()
Returns the nodal combination option for determining the nodal value for element and element-nodal results
License requirements: nx_masterfem ("Finite Element Modeling") OR nx_design_sim ("NX Design Simulation") . |
static PostGraphBuilder.NodalCombination |
PostGraphBuilder.NodalCombination.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static PostGraphBuilder.NodalCombination |
PostGraphBuilder.NodalCombination.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static PostGraphBuilder.NodalCombination[] |
PostGraphBuilder.NodalCombination.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
PostGraphBuilder.setNodalCombinationValue(PostGraphBuilder.NodalCombination nodalValue)
License requirements: nx_masterfem ("Finite Element Modeling") OR nx_design_sim ("NX Design Simulation") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.